Technical FAQs

Ask a Question

Customer has a Homeline loadcenter and the cover screws are too large.

The screws are thread forming type that will require extra force to install the first time. Suggest using #2 Robertson square tip screw driver.


CTA-ID : 2011480
Was this helpful?
What can we do to improve the information ?