Technical FAQs

Ask a Question

How do you run the auto diagnostic test on the 8803 unit?

1. The motor must be disconnected.
2. All the line power must be removed. Can only have control power to the unit.
3. With the power off the Auto Test switch should be turned on and unit powered back up then it will run the test.



CTA-ID : 2011478
Was this helpful?
What can we do to improve the information ?