Technical FAQs

Ask a Question

Can the 8940 Type S2 pump panels be modified to melting alloy type overload relay?

Yes, factory modification is available by ordering using Form Y61 for standard trip (Class 20) or Y611 for quick trip (Class 10)

CTA-ID : 2012005
Was this helpful?
What can we do to improve the information ?