Technical FAQs

Ask a Question

9012ACW2 crosses to either 9012GBW1 or 9012GEW1. Which one should he use?

The unit with the non-adjustable differential provides no option of adjusting the spread between the set points on the switch. The range can be changed but the other point of transition will always be the same value added to the range. The adjustable differential allows the spread to adjusted with in given limits.


CTA-ID : 2011999
Was this helpful?
What can we do to improve the information ?