Technical FAQs

Ask a Question

What is the maximum size and number of cables per phase for HVL/cc switches?

Two 500 kcmil cables per phase. (This is the maximum number per field shaper).

In a 20`` wide incoming section two field shapers per phase can be mounted on the bus. This will allow four 500kcmil cables per phase to be terminated.




CTA-ID : 2011833
Was this helpful?
What can we do to improve the information ?