Technical FAQs

Ask a Question

What can happen in the Product Selector if a rear connector assembly is chosen?

The selector is programmed to place rear connector assemblies on the Lineside and Loadside of the switch as required. If it is a single switch, then this is a problem if the cables are entering and exiting from the same direction, top or bottom.
It is probably best NOT to choose this selection unless the customer is insisting. The logic in the Product Selector places the rear connectors as required, based on cable size, cable entry and the number of cables per phase. Picking the rear connector option will add an extra section, if there is interference between the load and line side rear connectors.

CTA-ID : 2011829
Was this helpful?
What can we do to improve the information ?