Technical FAQs

Ask a Question

What is the maximum BIL available in the Product Selector?

The Maximum BIL is 150kV for HVL/cc. 110kV and 150kV HVL/cc require insulated bus. The maximum BIL is 95kV for HVL in the selector, but HVL also goes to 34.5kV 150kV BIL.

At the present time the HVL Product Selector is 17.5kV 95kV BIL maximum. The HVL/cc has voltages up to 34.5kV.

CTA-ID : 2011826
Was this helpful?
What can we do to improve the information ?