Technical FAQs

Ask a Question

AP14G busway is pending obsolescence. Will there be an adapter available to go from old AP to the new Powerbus 225?

No. To connect the two types of busway you will need to use cable tap boxes and then cable between the two systems.


CTA-ID : 2011673
Was this helpful?
What can we do to improve the information ?