Technical FAQs

Ask a Question

What is the specifications on the 24v dc power supply and the total available mA for the ATV58 Econo Flex unit?

The 24v control supply specifications is Minimum 20 V; Maximum 30 V; I = 140 mA.

Total current of +24v internala supply is 140mA.  If more current is required, an external supply must be used.

Each LI on unit is rated for 10 mA.


CTA-ID : 2011985
Was this helpful?
What can we do to improve the information ?