Technical FAQs

Ask a Question

Should the Detailed Pricing Sheets be checked?

Yes, the Detailed Pricing Sheets are the most important part of the Product Selector output.

***ALWAYS CHECK THE DETAILED PRICING!!!***

PLEASE BE SURE TO PRINT OUT THE DETAILED PRICING SHEETS. CLICK ON ``OTHER RESULTS`` TO PRINT DETAILED PRICING. VERIFY THAT ALL OF THE ITEMS YOU HAVE SELECTED HAVE BEEN PRICED. THERE COULD BE PRICING ERRORS IN THE SELECTOR.
DO THIS FOR EVERY QUOTATION !
CHANGES ARE MADE ALMOST DAILY TO THE PRODUCT SELECTOR
SOME CHANGES MAY HAVE UNKNOWN EFFECTS ON THE
DETAILED PRICING
COMPLICATIONS CAN OCCUR FROM CONFLICTING RULES, ACE LOGIC AND LOCKOUTS
PLEASE REPORT ANY ERRORS IMMEDIATELY TO
Andy Freck @ 615-844-8571 / frecka@squared.com
Ed Reader @ 615-844-8567 / readered@squared.com





CTA-ID : 2011824
Was this helpful?
What can we do to improve the information ?