Technical FAQs

Ask a Question

Can the configuration of the Product Selector be forced in certain ways? Transiton Sections - Depth - Rear Connector Assemblies?



THIS PRODUCT SELECTOR IS SELF-CONFIGURING WITH INCOMING SECTIONS AND BUS TRANSTION SECTIONS ADDED ONLY AS REQUIRED. ENTER ONLY WHAT YOU NEED AND LET THE SELECTOR DO THE REST. OTHERWISE - YOUR RESULTS WILL NOT BE CORRECT. The selector will attempt to make the switchgear taller, before it makes it wider! Cable bending radii, number of cables per phase, top/bottom -cable entry/exit and other mounted components are critical to the layout. Bus transitions cannot be selected manually and Rear Connector Assemblies are added as required. Adding Rear Connector Assemblies often has adverse effects on the selector rules and logic and cause your lineup not to configure properly.

CTA-ID : 2011820
Was this helpful?
What can we do to improve the information ?