Technical FAQs

Ask a Question

What are the dimensions and the weight on the ATV58HD28M2, ATV58HD33M2, ATV58HD46M2, ATV58HD54N4, ATV58HD64N4 or ATV58HD79N4?

The Width is 13.78 in (350 mm)
The Height is 25.59 in (650 mm)
The Depth is 11.97 in (304 mm)
The weight is 126 lb (57 kg)


CTA-ID : 2011664
Was this helpful?
What can we do to improve the information ?