Technical FAQs

Ask a Question

Which direction do you count on the ATV66 J9 and J32 connections from the power board to main control board to determine what is pin # one?

Pin number one starts on the right side of the connector and you count to the left increasing in number.


CTA-ID : 2011659
Was this helpful?
What can we do to improve the information ?