Technical FAQs

Ask a Question

Do we make a limit switch rated NEMA 4?

All of our limit switches are Nema 4 except the type XCM.

See Limit switch enclosure ratings Digest 172 page 19-3.


CTA-ID : 2011658
Was this helpful?
What can we do to improve the information ?