Technical FAQs

Ask a Question

What 25kV thru 38kV switches can we offer to the OEM?

Only the fully assembled HVL/cc switch is UL listed. The 25kV and 39kV HVL switches are not UL listed.


CTA-ID : 2011445
Was this helpful?
What can we do to improve the information ?