Technical FAQs

Ask a Question

What are the dial increments for adjusting a mag-gard breaker?

The F and K frames have seven increments; the L and M frames have 5 increments. The increments are not linear. The setting tolerances are -20% to +30% of the nominal values.


CTA-ID : 2011444
Was this helpful?
What can we do to improve the information ?