Technical FAQs

Ask a Question

What documentation would be good to use for part of the customer`s Owner`s Operation manual for the Econoflex?

30072-450-10 is the instruction bulletin
``Class 8839 ECONOFLEX Adjustable Speed Drive Controllers for HVAC and Pumping Applications, 1 to 100 HP, 460 V and 1 to 50 HP, 208/230 V``

It is also helpful to have the ``Keypad Display Programming Guide for ATV58 TRX AC Drives, VW3A58101``, bulletin number VVDED397047.

These manuals are available for download at

CTA-ID : 2011977
Was this helpful?
What can we do to improve the information ?