Technical FAQs

Ask a Question

What is the part number for remote keypad kit and cable used on the Altivar ATV66?

VW3A66100 , 2 meters, or VW3A66101 , 3 meters ,
These kits include the mounting hardware and cable. They do not include the keypad. The existing keypad that is included with the drive can be used in this kit.


CTA-ID : 6896
Was this helpful?
What can we do to improve the information ?