Technical FAQs

Ask a Question

Where is the Serial number located on the Altivar ATV58?

There is a sticker with bar code on the Right side of the drive on the heatsink. The serial number is on that sticker.

CTA-ID : 2011810
Was this helpful?
What can we do to improve the information ?