Technical FAQs

Ask a Question

What is the difference between the standard 9998DA coils and the premium 9998DP coils?

The standard coils are supplied with Class B insulation rated 155 degrees Celsius. The premium coils are supplied Class H insulation rated 180 degrees Celsius.


CTA-ID : 2011807
Was this helpful?
What can we do to improve the information ?