Technical FAQs

Ask a Question

What type of nameplate is use on the 9001KY100/200 security stations?

Nameplate not available as a replacement.
Requires complete disassembly of the control station
Entire switch would have to be disassembled and re-assembled - not recommended.


CTA-ID : 2011805
Was this helpful?
What can we do to improve the information ?