Technical FAQs

Ask a Question

What are the weights and dimensions of the 8804 CT, EVT, or VT drives?

The size and weight of these products varied based on the enclosure style (e.g., disconnect, bypass, stand alone) and power ratings.
Refer to the appropriate service bulletin for dimension using the attachment links.
These drives have been obsolete since the mid to late 1990s. Therefore, not all literature is available in electronic form.

CTA-ID : 2011645
Was this helpful?
What can we do to improve the information ?