Technical FAQs

Ask a Question

Need to confirm the fault that expect to see when have current sensors that have date codes in 1997 which were informed during training had possible issues.

There is not a particular fault that would occur but would identify that the +/-15v supply was being pulled down.

Due to the design and build of the current sensors they could actually short to ground and pull down the supplies.
The majority of 1997 this issue occurred bust mostly from June to December date code.

CTA-ID : 2011637
Was this helpful?
What can we do to improve the information ?