Technical FAQs

Ask a Question

In a Q22200NRB enclosure there is a 2/0 lug on the ground bar but customer needs 3/0 lug and he is running aluminum wire, is there another lug that can be put in this enclosure?

You cannot put a lug to handle 3/0 lug on the ground bar.

CTA-ID : 2011440
Was this helpful?
What can we do to improve the information ?