Technical FAQs

Ask a Question

What is the enclosure rating for the ATV11 unit?

The unit is rated for IP20 degree of protection.


CTA-ID : 2011434
Was this helpful?
What can we do to improve the information ?