Technical FAQs

Ask a Question

8839 ATV66 What is board # 52013-082-50? This is installed in an old Enclosed drive from Columbia.

This is an early version of the 24VDC I/O extension module (VW3A66201T). It was designed an built in Columbia, and was used until the I/O card was released for sale. It was designed to have the same terminal strip and wiring as the I/O card, and should not require any rewiring to replace.


CTA-ID : 2011971
Was this helpful?
What can we do to improve the information ?