Technical FAQs

Ask a Question

What are dimensions and weight of an RL13001 line reactor?

11.25 inches wide
7.25 inches high
6.38 inches deep
It weighs 29 lbs. A detailed drawing can be found at

This is the part number for the open style reactor. An enclosed type is also available.

CTA-ID : 2011966
Was this helpful?
What can we do to improve the information ?