Technical FAQs

Ask a Question

What are the specifications on the ATS48 R2 relay?

This is a dry contact labeled R2A to R2C.
It is NO normally open non programmable contact.

The minimum switching capacity: 10mA for 6 Vdc
Maximum switching capacity on inductive load
   * 1.8 A for 230 Vac and 30 Vdc
   * Maximum voltage 400Vac.

CTA-ID : 2011962
Was this helpful?
What can we do to improve the information ?