Technical FAQs

Ask a Question

What is the size/type of fuse used in the DF6AB10 fuse holder?

It is 0.4`` X 1.5``  or 10mm X 38mm.


CTA-ID : 2011802
Was this helpful?
What can we do to improve the information ?