Technical FAQs

Ask a Question

What are dimensions and weight of an RL13003 line reactor?

11.25 inches wide
8.5 inches high
8.5 inches deep
It weighs 64 lbs. A detailed drawing can be found at www.mtecorp.com

This is the part number for the open style reactor. An enclosed type is also available.


CTA-ID : 2011788
Was this helpful?
What can we do to improve the information ?