Technical FAQs

Ask a Question

What is the range of current limit setting on the ATS46 units?

It is adjustible from 150 to 700% of In setting. However, maximum is limited to 500% of rated softstarter current.

CTA-ID : 2011622
Was this helpful?
What can we do to improve the information ?