Technical FAQs

Ask a Question

Is the part number VW3A58355U that the digest 172 on page 24-5 have listed for the Ethernet Modbus TCP/IP Communication Card correct?

No. The Digest 172 had the incorrect part number listed.
The orderable part # is VW3A58310U.


CTA-ID : 2011619
Was this helpful?
What can we do to improve the information ?