Technical FAQs

Ask a Question

Can the analog outputs for the ATV58 with I/O extension cards be set up with different scaling for each output?

If using the Analog I/O card VW3A58201U or Digital I/O card VW3A58202U, the answer is no. Both the AO and AO1 will have the same scaling factor as set in Menu #4 parameter AOL and AOH.

If the customer is using the VW3A58253 GPO the AO1, AO2 and AO3 on the card can be set for different values.

See the instruction bulletins for the individual option cards for details.

CTA-ID : 2011210
Was this helpful?
What can we do to improve the information ?