Technical FAQs

Ask a Question

Why does the unit not operate when wired like the recommended diagram on page 75 of the June 2002 ATS48 manual.

The user`s manual recommended diagram on page 75 is incorrect for proper operation.  
On line 3 of the ladder diagram where you see the NC FR relay contact in series with the RCR and IC coil.  The NC FR should actually be a NO (normally open) FR contact.

This configuration would then allow proper operation of unit.

CTA-ID : 2011414
Was this helpful?
What can we do to improve the information ?