Technical FAQs

Ask a Question

What is the recommended shorting contactor part number for the ATS48C41Y

LC1F400 is rated for AC1 duty for shorting contctor.
A larger contactor may be used if it is to be used for full voltage bypass. Base the contactor size on the motor FLA.

NOTE: This contactor requires lugs for the line and load terminal connections.


CTA-ID : 2011777
Was this helpful?
What can we do to improve the information ?