Technical FAQs

Ask a Question

Are there lugs that will accept #1 copper conductors on an MA36600?

Not for branch-feeder applications. A 600 A breaker will not protect #1 awg wire.

For UL 508 applications:
A PDC6MA20 will accept 6 #12 to 2/0 copper
PDC12MA4 will accept 12 #14 to #4 copper


CTA-ID : 2011776
Was this helpful?
What can we do to improve the information ?