Technical FAQs

Ask a Question

Customer asks if the 8501CO16V20`s coil is 120v 50/60Hz rated?

Class 8501 Type C are AC Voltage 50/60 Hz rated.



CTA-ID : 2011608
Was this helpful?
What can we do to improve the information ?