Technical FAQs

Ask a Question

Are the sub feed lugs included in the NQOD442L600TFL interior?

No, this is a thru-feed panel. Main sub-feed lugs are not available on 600A interiors.


Revised 4/27/04



CTA-ID : 2011406
Was this helpful?
What can we do to improve the information ?