Technical FAQs

Ask a Question

What is the part number for the ATS46 C32N bypass contactor.

If referring to the shorting contactor that pulls in when motor is up to speed the part # is LC1F330G7.


CTA-ID : 2011405
Was this helpful?
What can we do to improve the information ?