Technical FAQs

Ask a Question

What is the maximum distance the Altivar ATV66 keypad can be remotely mounted.

We provide a 3 meter ( approximately 10 feet ) cable which is the maximum available from SquareD.
Some people have made their own cables that are longer than 3 meters. If this is done, we can not guarantee that it will work reliably.


CTA-ID : 2011941
Was this helpful?
What can we do to improve the information ?