Technical FAQs

Ask a Question

Can the ATS48 be run continuously across the line after the motor is up to speed?


You can keep the softstart on line if desire or can supply shorting contactor to pull in once the unit is up to speed to allow for less watts loss and increased life expectancy on the SCRs while the starter still provides protection for motor.

CTA-ID : 2011771
Was this helpful?
What can we do to improve the information ?