Technical FAQs

Ask a Question

Can the HVL/cc switch be purchased with provisions only for fuses?

Issue:
Can the HVL/cc switch be purchased with provisions only for fuses?

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Application.

Resolution:
Yes, the HVL/cc switch could be provided with fuse clips only making the provisions for fuses to be added. DIN/E fuses will have to be used.

DIN/E fuses are manufactured for Square D by Cooper Bussman.


CTA-ID : 2011598
Was this helpful?
What can we do to improve the information ?