Technical FAQs

Ask a Question

Is the HVL standard N3R roof one piece?<br />Is it welded?

Yes, the standard HVL roof for outdoor N3R is one piece.

It is not welded. The roof has flanges on the sides which turn up and then are covered by roof rabbets.

CTA-ID : 2011596
Was this helpful?
What can we do to improve the information ?