Technical FAQs

Ask a Question

How do I change the LSP on the ATV66?

Carefully place your hand in front of the keypad and using a small flat blade screwdriver on top of the keykpad snap the keypad by depressing the tab.
On the back side of the keypad there is a switch that has to be in the unlock position. Once the keypad is unlocked and if not in keypad command mode press the F3 key which is the GoTo Menu key and enter in 10.0 and move the pointer to the Total Unlock position and then press Enter.
Press the F3 key again and Go To Menu 1.0 and then you move down the menu to the appropriate parameter and make your changes.

Reverse the process to lock the software and keypad to avoid any changes by unauthorized operators.

CTA-ID : 2011593
Was this helpful?
What can we do to improve the information ?