Technical FAQs

Ask a Question

Individual and ganged meter sockets feature 10KA short circuit rating. What does ``or higher with Utility approval`` mean?

The device is UL listed at 10K. Utilities may test a device and accept it for higher ratings, but it will not be UL listed.

CTA-ID : 2011933
Was this helpful?
What can we do to improve the information ?