Technical FAQs

Ask a Question

Do NQOD panelboards have a split neutral?

100 - 225 A interiors have a split neutral located on the same end as the mains.

400 - 600 A interiors have a neutral (not split) located on the end opposite the mains.


Revised 4/13/04


CTA-ID : 2011932
Was this helpful?
What can we do to improve the information ?