Technical FAQs

Ask a Question

What will cause a 38kV HVL/cc switch section to be 39.97`` (1000mm) wide rather than 29.50`` (750mm) wide?

Items which will cause a 38kV HVL/cc switch section to be 39.97`` (1000mm) wide rather than 29.50`` (750mm) wide.

Fuses above 65E are double barrell and require a wider section of 39.37`` (1000mm).

Fused switch sections with surge arresters on the load side will require a wider section of 39.37`` (1000mm).




CTA-ID : 2011925
Was this helpful?
What can we do to improve the information ?