Technical FAQs

Ask a Question

What are the switching capabilities of the HVL/cc switch, both 600A and 1200A? (Electrical and Mechanical Endurance)

Endurance of HVL/cc switches:

600A 1000 operations at No Load
100 operations at Full Load
1200A 1000 operations at No Load
26 operations at Full Load


CTA-ID : 2011922
Was this helpful?
What can we do to improve the information ?