Technical FAQs

Ask a Question

What main breaker is used in the 2000A EZM main breaker devices, both single and three phase?

Issue:
Current product design

Product Line:
EZM Metering

Environment:
Main Breaker

Cause:
Applicaton

Resolution:
Single Phase EZM12000CB and EZM12000CBU mains are each supplied with a factory installed RJF26200 circuit breaker.
Three Phase EZM32000CB and EZM32000CBU mains are each supplied with a factory installed RJF36200 circuit breaker.

Both of these 2000A Type RJF circuit breakers are 80% Rated and are NOT supplied with changeable rating columns or adjustable ampere rating dials.



CTA-ID : 2035206
Was this helpful?
What can we do to improve the information ?