Technical FAQs

Ask a Question

What is the heat dissipation for the ATV58HC19N4XZU drive at rated load?

The Dissipated power for this drive is 4000 Watts at rated load.
See the Instruction Bulletin VVDED397048US ALTIVAR 58 TRX Adjustable Speed Drive Controllers Installation Guide for Type H Controllers for additional mounting and cooling guidelines.


CTA-ID : 2011912
Was this helpful?
What can we do to improve the information ?